Create a Data Snapshot for network training

In order to start the training of a network, a Data Snapshot needs to be created which contains the annotated images. A Data Snapshot is a point in time snapshot of the data in your domain. This means that if you add, remove or edit annotations, you need to create a new Data Snapshot in order to include those changes.

create snapshot

Give the Data Snapshot a name which makes it easy to distinguish it from others in the future. It could include the date or other information describing the changes compared to the previous Data Snapshots, eg. "Added pasta from station 2".