Skip to content

Deploying networks in SICK Nova

In order to run your trained network on a device, please open up the browser on your PC and enter the IP of your SICK device in order to access the SICK Nova UI. If you are unfamiliar with using SICK Nova, please see this tutorial series on YouTube (part 1 and part 2 are recommended).

Currently supported SICK devices:

  • Inspector83x (monochrome and color devices)
  • Inspector85x

Please note that the Intelligent Inspection license is needed to gain unlimited access to both the AI Object Detection (dStudio) tool and the AI Blob Finder (dStudio) tool.

Downloading a network model from dStudio

After you are happy with the evaluation results you can go to the Deployments tab to find an overview of the models that you have trained. Press the Get Model button and choose if you want to run download a trial version of the network (can be run up to two hours) or purchase a network. You can learn more about trial mode on the dStudio start page.

Get Model

Deploying in Nova

The dStudio Object Finding networks are deployed in the AI Object Detection (dStudio) tool for object detection, and the AI Blob Finder (dStudio) tool is used for instance segmentation in SICK Nova. How to do so is described in the Operating Instructions, which can be downloaded from the Nova Inspector product page on sick.com, as well inside of the tool by clicking the blue question mark icon.